Other Parts Discussed in Thread: TMS320F28335
Hi
I am using the TMS320C2000 (F28335) Development Tool and CCSv4 in a project, where I need store a couple of large arrays on the RAM of the DSP. Therefore I have tried enlarging the RAML6 section in the linker file (28335_RAM_lnk.cmd). Here is the changes I have made:
====== BEFORE ======
PAGE 1 :BOOT_RSVD : origin = 0x000002, length = 0x00004E
RAMM1 : origin = 0x000400, length = 0x000400
RAML4 : origin = 0x00C000, length = 0x001000 RAML5 : origin = 0x00D000, length = 0x001000
RAML6 : origin = 0x00E000, length = 0x001000
RAML7 : origin = 0x00F000, length = 0x001000
ZONE7B : origin = 0x20FC00, length = 0x000400
====== AFTER ======
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x00004E
RAMM1 : origin = 0x000400, length = 0x000400
RAML4 : origin = 0x00C000, length = 0x001000
RAML5 : origin = 0x00D000, length = 0x001000
RAML6 : origin = 0x00E000, length = 0x200C00
RAML7 : origin = 0x20EC00, length = 0x001000
ZONE7B : origin = 0x20FC00, length = 0x000400
==================
Also, in order to make sure that the arrays (of doubles) are placed in the RAML6 section (called ".toRAML6") , I have made the following above my main.c file:
#pragma DATA_SECTION(Table1, ".toRAML6");
#pragma DATA_SECTION(Table2, ".toRAML6");
#pragma DATA_SECTION(Table3, ".toRAML6");
double Table1[BufferSize];
double Table2[BufferSize];
double Table3[BufferSize];
==================
Because this gave the error "memory map prevented read of target memory......" when trying to access the tables from the Watch window, I found some inspiration on the Internet regarding changes in the "f28335.gel" file, which is used for the project. In the file I just changed the sizes of the RAM sections according to those in the linker file:
hotmenu F28335_Memory_Map()
{
...
/* Program memory map */
...
GEL_MapAdd(0xE000,0,0x200C00,1,1); /* L6 SARAM */
GEL_MapAdd(0x20EC00,0,0x1000,1,1); /* L7 SARAM */
...
/* Data memory map */
...
GEL_MapAdd(0xE000,1,0x200C00,1,1); /* L6 SARAM */
GEL_MapAdd(0x20EC000,1,0x1000,1,1); /* L7 SARAM */
...
}
hotmenu Fill_F28335_RAM_with_ESTOP0()
{
...
GEL_MemoryFill(0x00E000,1,0x201C00,0x7625); /* Fill L6/L7 */
...
}
==================
This cancelled the error, but I am still not able to use some of the memory in the RAML6 section. When using a "BufferSize" of, say, 2000 everything works. However, when increasing the "BufferSize" to 5000, none of the entrances in the arrays get updated at all and all I get is af bunch of zeros in the arrays. And there is no error messages or what so ever.
Can anyone help explaning what I have done wrong? And how to fix it?
Best regards,
Morten.