Other Parts Discussed in Thread: TMS320C5515, MSP430G2231
hi,
i had a kit msp430g2231, but i did not install the file "setup_CCS_MC_Core_4.2.0.10018", which comes along with i kit. I, however, installed the file "setup_CCS_4.1.0.02002", which comes along with the kit tms320c5515. When i do project with msp430g2231, the code composer studio cannot debug.
this is the message: Error initializing emulator:
Unable to locate entry point for MSP430_GetNumberOfUsbIfs
plz show me way to fix it.
thank,