This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use different sets of expressions according to the open project ?

Hi,

I used to work with IAR and have some projects on CCS9 now.

On IAR when you want to open a workspace you can click on the .eww file and get your workspace with 1 or more projects and the watch windows containing dedicated expressions that you added.

What is the way on CCS ?

For example I have one C2000 project with a set of expressions, then I need to work on a MSP430 project with an other set of expressions.

- do I need to import/export the expressions every time ? (not the best way because it adds the imported expressions to the current set instead of replacing it)

- should I use the switch workspace option ?

- Is there an other way ?

Thank you.

Best regards, Romain

  • Hello Romain,

    RomainP said:

    - do I need to import/export the expressions every time ? (not the best way because it adds the imported expressions to the current set instead of replacing it)

    - should I use the switch workspace option ?

    Either one of these options would work.

    The second option is likely the preferred one for your use case

    Thanks

    ki