Part Number: PROCESSOR-SDK-AM437X
Hello,
I am using the SDK example project "QSPI_BasicExample_idkAM437x_armExampleProject". According to my understanding there is a 512[MBit] = 64[MByte] QSPI flash in use on the AM437x IDK.
Is it possible that the flash size hash #define in the QSPI NOR Flash driver is wrong?
It looks like the hash defines indicates a 32[MByte] flash.
The code above is also valid for the newer SDK version 6.3.0.106.
Thanks,
Inno