Part Number: CCSTUDIO-SITARA
Other Parts Discussed in Thread: AM5749
I am using CCS ( Version: 10.1.1.00004) in Windows for the AM5749 target with the processor_sdk_rtos_am57xx_6_03_00_106 sdk.
It seems all of the "Software" subtitled resource packages are for targets other than AM57xx. Though C2000, CC26xx, CC32xx, MSP432x4 and Sitar AM335x, AM437x and AM1C110 seem prolific, a casual search using the filters features yields NOTHING for the AM5749 (or any AM57xx).
Is there an update or addend I need to download and install in order to see AM5749 in the Resource Explorer?