This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

undefined reference to main in gcc V9 assembly code (and not only ...)

Hi all,

I leave CCS for a while and I'm back to CCS V10 (latest version) on Windows 7 64bits, for a simple project using gcc V9 (latest version) in assembly code.

I'm a bit disappointed ;-)

The following file (test.S, the only file of project) :

-----------------------------------------------------------------

.text

Reset:

jmp Reset

.section .resetvect,"ax",@progbits

.word Reset

-----------------------------------------------------------------

generate the following errors during link time (compile is ok ;-) )

---------------------------------------------------------------

makefile:144: recipe for target 'test.out' failed

c:/ti/ccs1010/ccs/tools/compiler/msp430-gcc-9.2.0.50_win64/bin/../lib/gcc/msp430-elf/9.2.0/../../../../msp430-elf/bin/ld.exe: test.out section `__reset_vector' will not fit in region `RESETVEC'

c:/ti/ccs1010/ccs/tools/compiler/msp430-gcc-9.2.0.50_win64/bin/../lib/gcc/msp430-elf/9.2.0/../../../../msp430-elf/bin/ld.exe: region `RESETVEC' java-scripted by 2 bytes

c:/ti/ccs1010/ccs/tools/compiler/msp430-gcc-9.2.0.50_win64/bin/../lib/gcc/msp430-elf/9.2.0/../../../../msp430-elf/bin/ld.exe: c:/ti/ccs1010/ccs/tools/compiler/msp430-gcc-9.2.0.50_win64/bin/../lib/gcc/msp430-elf/9.2.0/../../../../msp430-elf/lib\libcrt.a(crt_main.o): in function `.Loc.254.1':

(.crt_0800call_main+0x4): undefined reference to `main'

------------------------------------------------------------

Where am I wrong ?

Claude