Other Parts Discussed in Thread: TMS320F2806, TMS320F2812
SIR,
I HAVE XDS510PP PLUS JTAG AND ALSO CCS 3.1 STUDIO.
I JUST WANTED TO PROGRAMMING MY FLASH OF 2812 AND 2806 DIRECTLY BY CCS 3.1 STUDIO.
PLEASE INFORM ME.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F2806, TMS320F2812
SIR,
I HAVE XDS510PP PLUS JTAG AND ALSO CCS 3.1 STUDIO.
I JUST WANTED TO PROGRAMMING MY FLASH OF 2812 AND 2806 DIRECTLY BY CCS 3.1 STUDIO.
PLEASE INFORM ME.
Hi,
With a risc of not understanding what you actually want to do....
I have CCSv4, don't know how much difference there is from 3.1 but anyway, this is how I would do it:
1. Build my application with a linker command file specifying flash as program memory
2. Create a target configuration for the XDS510 and DSP
3. Switch to "debug mode" and connect to your tagret (In CCSv4 this would be Target->Connect Target
4. Once connected, Load your app (in CCSv4 Target->Load Program)
/Ola
Hi, Darshit,
You first check whether CCS3.1 on-chip flash programmer can support F2806, which should support F2812. If yes, you can use the plug-in tools, F28xx on-chip flash programmer to program the flash (Tools->F28xx on-chip flash programmer).
Best Regards,
Yanming
hi Yanming,
first of all thanks for reply,
CCS3.1 on chip flash programmer is supporting to F2806/08, F2810/11/12.
but i am unable to find option for on chip programming. ( Tools->>on-chip flash programmer.)
is it like that once we must have to add linker command file for flash and then this on-chip flash programmer will highlighted in Tools manu.
Darshit.
darshit prajapati said:hi Yanming,
first of all thanks for reply,
CCS3.1 on chip flash programmer is supporting to F2806/08, F2810/11/12.
but i am unable to find option for on chip programming. ( Tools->>on-chip flash programmer.)
is it like that once we must have to add linker command file for flash and then this on-chip flash programmer will highlighted in Tools manu.
Darshit.
I'm not sure why the flash programmer is not showing up under the tools menu. I am going to move this to the code composer forum to see if they have any ideas.
Regards,
Lori
Darshit - The C2000 flash programmer does not come with the default CCS 3.1 installation. You need to install an additional plug-in:
https://www-a.ti.com/downloads/sds_support/C2000FlashPlugin.htm
Thanks
ki
THANK YOU VERY MUCH K-SOO LEE,
your link is really great full help to me.
thank you very much.,
lee i just wanted to know that i have DSP TMS320F2806 AND TMS320F2812 BOARD.
I JUST WANTED TO PROGRAMM THAT BOARD VIA/THROUGH MATLAB.
IS IT POSSIBLE? IF YES THEN PLEASE LET ME KNOW HOW? PLEASE
IF POSSIBLE GIVE ME ANY EXAMPLE IF IT IS IN YOUR MIND.
THANKS VERY MUCH.
I know that Matlab supports CCS 3.x so it should be possible. I don't have much knowledge beyond that. You should contact The Mathworks support for more help.
ki
Target support is available for many members of the C2000 family through MathWorks Target Support Package and Embedded IDE Link tools.
For an overview of how this functionality works, check out http://www.mathworks.com/c2000
Regards,
-noam
thanks Noam,
thanks very much,
i go through link what you had provided and its really good link give me more clearity.
please gime me more link related to TMS320F2812/TMS320F2806 related help(if possible)
thanks Noam, thanks very much again.
regards,
Darshit
Hello,
I am struggling with the issue to find the 'on chip processor' in the tools in CCS3.1 version. I downloaded the flash programmer that supports TMS320F2812 and put that in the CCS3.1 folder.
How will I get the 'on chip flash programmer' in the tools menu in CCS3.1
Regards,
Sherly
Hello Sherly,
I got help from ki in previous conversion. I am repeating for your ready reference once again.
"Darshit - The C2000 flash programmer does not come with the default CCS 3.1 installation. You need to install an additional plug-in:
https://www-a.ti.com/downloads/sds_support/C2000FlashPlugin.htm
Thanks
ki"
I had downloaded Flash Plugin and installed in machine with CCS 3.1. After installation of plugin you will be able to see and access the "on chip flash programmer" tab under tool.
Regards,
Darshit
I had checked link for plug in. I was downloaded plug in for V3.1 and its working fine.
What is your specific requirement ( which version are you use for CCS and also for which controller?)
If it is suitable then I will upload it and share link to you.
Regards,
Darshit.
Hello,
darshprajapati@yahoo.co.in has sent you a file that will EXPIRE in 3 days.
To view and download your files, visit:
www.sendthisfile.com/rqjVr3i9BuL58WGVCanKWJC5
File:
C2000FlashPlugin1.13.0.exe