Part Number: TMDSICE3359
Hi,
I downloaded CCS9.3 from software-dl.ti.com/.../index_FDS.html and I installed it to a laptop which earlier had only Windows 7 but now only Ubuntu 18.04 but it seems that there is a display driver issue because it quite often goes black but it is only annoying when using terminal or web browser but it seems that CCS9.3 exits or at least does not start properly as can be seen in a video I uploaded to Dropbox in www.dropbox.com/.../IMG_0478.MOV. Is this something which is fixed in CCSv10 or should I find another computer running 64-bit Linux?
Regards,
Jani