Other Parts Discussed in Thread: TMS320C5515
I purchased TMS320C5515 EVM and want to test the ECG System v 5.7 (from the CD). I imported the project using Import Legacy CCSV3.3 Project, Connected the board using USB cabel, now when i try to build the project it gives the following error
subdir.mk:56: *** target pattern contains no `%'. Stop.
and a message appears saying that it can't find the .out file, and the file exists in the folder.
Any help for this, can I download the CCS V3.3?
Thanx