Part Number: PROCESSOR-SDK-DRA8X
Tool/software: TI C/C++ Compiler
Hi Karan,
My previous thread for SBL is here : https://e2e.ti.com/support/tools/ccs/f/81/t/975865
I'm able to boot using SBL, now same application.out is not booting with SPL. (Using PSDK7.0)
I have prepared SDCard for Linux and keeping application.out in /lib/firmware/pdk-ipc/ path in the SDCard and doing soft link ( sudo ln -sf /lib/firmware/pdk-ipc/application.out j7-mcu-r5f0_0-fw ).
As per my understanding, if we keep as mention above then SPL will boot application.out. Let me if I'm wrong.
Can you please give your input/suggestion for the below logs ?
Please find below linux boot logs.
======================================================
U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 15:08:08 +0000)
SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
Remoteproc 2 started successfully
Starting ATF on ARM64 core...
NOTICE: BL31: v2.3():07.00.00.005-dirty
NOTICE: BL31: Built : 14:33:55, Jun 17 2020
U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000)
SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla')
ti_sci_power_domain_on: get_device(197) failed (-19)
ti_sci_power_domain_on: get_device(197) failed (-19)
ti_sci_power_domain_on: get_device(197) failed (-19)
Trying to boot from MMC2
ti_sci_power_domain_on: get_device(92) failed (-19)
spl: could not initialize mmc. error: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
======================================================
Thanks,
-Makani