Other Parts Discussed in Thread: CCSTUDIO
This is almost certainly an Eclipse issue, however I thought I'd ask in this forum to see if anyone has come across a solution.
Since upgrading to Big Sur (I just realized CCS10 is not yet supported on Big Sur), I can no longer move and dock ANY window within CCS (Eclipse). Grabbing any window tab (e.g., open editors, Outline, Call Hierarchy, etc.) and trying to drag it has no effect - the window will not move or detach. It is possible to right-click on a window tab and select Detach, but then it is not possible to dock the detached window anywhere.
I am running CCS 10.1.1.00004, and I am not certain if Eclipse installs and uses its own Java JRE or if it relies on the system one (I'm assuming the former). Java on my Mac is /usr/bin/java and is version 1.8.0_151.
Has anyone else seen this and come across a solution or a place to research it? I have found very little on the web about this, which I find amazing if this is a class problem with Eclipse/Big Sur.
Thanks!
-Mark