I downloaded a led_ex1_blinky from the resource explorer available in the ccs 8.3.1. as shown in the following figure. When I try to compile it, it gives me me 'gmake: *** No rule to make target 'clean'' error and does not compile. How can I solve this issue? I deleted all previous CCS and reinstall clean ccs 8.3.1 to resolve this issue which did not help. Can I get suggestions to solve this issue?
This led_ex1_blinky example is an example code for the TMS320F28379D device.