In our custom board we use DP83822IFRHBR PHY for EtherCAT. COL pin of the PHY is used to determine the PHY address at PHY reset (strap). There is 3.3 volts at the COL pin during PHY reset when COL pin is not connected to any other device or resistor, as expected. However, there is only about 1 volt at the COL pin during PHY reset when COL pin is connected to RXLINK pin (pin E24) of the AM4377. RXLINK is an input pin with pull up. We also tried to configure E24 pin as gpio5_13 input with pull up, but with the same result. What can be the cause for this behavior? Is there anything we should check or do to overcome this issue?