Dear all,
I'm developing an application on 674x DSP platform. I'm using code composer studio 4.2. My code compiles fine without "program mode compilation" option enabled. But when I turn on the "program mode compilation" -pm option for optimization, the code doesn't compile anymore. I noticed that -pm option works if I provide a single file. When I add folders to the project the code doesn't compile anymore. Can anyone help me with this issue.
Regards,
Asif Jalaludeen,
TU Delft