Part Number: MSP430F5328
Other Parts Discussed in Thread: UNIFLASH
Hi everyone!
I am using CCS ( Version: 8.2.0.201809041400 ; Build id: N201809041400 ) to download a TI-txt file into the device using USB FET.
- 1 - I tryed with "Run / Load / Select Program to Load" , but nothing happens ( without any open project : all closed in Project Explorer)
- 2 - If there is an opened project then "Run / Load / Select Program to Load" works and it lets me choose the txt file. But the download fails.


- 3 - Trying to download the txt file using elprotronic sofware and the USB FET all works perfectly.
- 4 - Trying to download the same txt file using the gang programmer from texas all works perfectly.
- 5 - Debugging the opened project works perfectly (but it has a different txt file!).
Could be I am making some stupid error?
Is there something wrong with the txt file format? Here it is: