Other Parts Discussed in Thread: UNIFLASH, LAUNCHXL-CC26X2R1
Hi,
I am facing issue in flashing/debugging TI-Lauchpad, earlier it was suggested to perform the mass erase to resolve the issue, but we are unable to perform mass erase using both uniflash and ccs
we are getting below error while performing mass erase using uni flash.
in CCS we did not find scripts to perform mass erase, and unable to establish connection with lauchpad. logs attached.
[Start: Texas Instruments XDS110 USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\xj682d\AppData\Local\TEXASI~1\CCS\
ccs1020\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Jan 1 2021'.
The library build time was '11:25:57'.
The library package version is '9.3.0.00032'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-242' (0xffffff0e).
The title is 'SC_ERR_ROUTER_ACCESS_SUBPATH'.
The explanation is:
A router subpath could not be accessed.
The board configuration file is probably incorrect.
[End: Texas Instruments XDS110 USB Debug Probe]
Regards,
Cibi