Other Parts Discussed in Thread: SYSCONFIG
I'm currently developing a CC3235 application. I previously had CCS 10.2.0 and SDK 4.40 installed, then decided to update to CCS 10.3.0 and SDK 5.10.
I have CCS 10.3.0 installed and compiling fine. I also installed SDK 5.10 in its usual location (C:\TI\simplelink_cc32xx_sdk_5_10_00_02). I wanted to import an I2C example from SDK 5.10, so I went into TIREX to do that. Here's the example selected:

However, when I try to import it, TIREX insists that some additional packages need to be installed... namely SDK 5.10 (already installed) and SysConfig 1.8.0 (installed as part of CCS 10.3.0).

However, CCS itself sees no issue and recognizes that SDK 5.10 and SysConfig 1.8.0 are both installed:

So... what gives? Why is TIREX refusing to recognize the installation of SDK 5.10 and SysConfig 1.8.0?
David R.