Tool/software: TINA-TI or Spice Models
Hi,
Is it possible to design 3 output winding transformer on TINA-TI ?
If yes, How do I do that?
Thanks
Go
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Go,
If you call "ideal transformer", you can just put the primaries in parallel, as shown below:
You an also do it with Coupled Inductors, as shown below. The source "sees" the parallel of the two secondaries inductance (ignoring any current related to the secondary load). So, I believe in effect the the combination of the two coupled inductors connected this way, behaves the same as three coupled inductors.
Here are the two respective TINA-TI files for reference:
Ideal transformer two secondaries 3_2_17.TSC
coupled inductors two secondaries 3_2_17.TSC
Regards,
Hooman
Hi Go,
I forgot to mention that for the coupled inductor case:
a) Primary input impedance: The top trace is the current through a small resistor placed in series with the source to read the current (+/-3.16mA) to verify the loading on the source. I later removed this resistor (R4) which is not in the TINA-TI files I shared.
b) Simulation Start: I had to run the simulation Start for a long time to make sure the transients have settled (that's why the long simulation time) because I wanted to ensure the DC "average" source current is 0 (as it should be when only driving two transformers).
c) Simulation Artifact / Convergence: The other very small resistors (R3, R5) in series with the coupled inductor windings were needed for TINA-TI to converge. They don't serve any purpose for the circuit (just for simulation).
Regards,
Hooman
Hi Go,
One more thing.
I think it's easier to follow the method that my colleague Britt Brooks has recommended here as "subcircuit import" to build a transformer with arbitrary number of secondaries:

Regards,
Hooman