Tool/software: WEBENCH® Design Tools
I'm evaluating a quite old and probably poorly optimised design that uses LM2735Y with input 4.38V-5.25V, output 5.835V at 0.12A. Changing the default WEBENCH design to use our actual components is hampered by some apparently odd restrictions.
A simple but relatively unimportant example is with the feedback resistors, which default to 36.5k and 10k, both in 0201 packages. If I change these to our values of 51.1k and 14k by editing the limits in the Alternate Part Selection dialogue, the alternates offered all have the correct value but only in 0805 packages or larger - why is that? (We actually use 0603 in this case.)
A more frustrating issue is with some of the capacitors. Cin defaults to a 2.2uF X7R ceramic, but the list of alternates (without editing any limits) includes the 10uF X5R part that we actually use (TDK C1608X5R1A106K080AC), so that's fine. On the other hand, Cout defaults to a 47uF tantalum (in spite of the datasheet recommending ceramics!), where our design uses 3 off 10uF X5R, the same part as we use for Cin, but even if I edit the limits I cannot persuade the Alternate Part Selection dialogue to offer this choice. Obviously I can 'create a custom part', and doing it that way suggests that our design is seriously off optimum in this area, with a very low phase margin. However that's an inconvenient method because I have to find out and apply the derating of capacitance value with DC voltage manually, rather than letting WEBENCH do it, which it seems to do very well for standard parts that it knows about. Since WEBENCH allows this part for Cin, why can I not select it for Cout?