Other Parts Discussed in Thread: TPS62740
Tool/software: WEBENCH® Design Tools
When in 'Simulate' frame: When making a change to the Vout of the DC/DC, using the 'Change' menu item in the top line, the resistor values do not update on the schematic shown in the simulation window, nor do the Vin parameters shown update on this schematic...
so, here it is for 3.3 V, with 309k Rfbt
Now, changed to 2 V Vout, as shown in the top line, but Rfbt is still showing 309k
And, it seems that Vin values do not change correctly, either...