Part Number: THVD8000EVM
Other Parts Discussed in Thread: THVD8000
Tool/software: WEBENCH® Design Tools
Dear Sir,
We have completed the testing of 2 EVM Board of THVD 8000 and its working fine as per our application.I have some query while testing the THVD in real application.
The actual process will be like. Data will flow through Ethernet to Uart then to the first node (THVD 8000) on DC bus.Only 2 wires will be coming out from the converter or gateway
For this converter we need To put thvd8000 IC on the master side so that uart single will be converter to THVD8000 signal with Signal A and Signal B superimpose on DC power.Which included the components which are marked below in the pic. (Like