Part Number: THVD8000EVM
Other Parts Discussed in Thread: THVD8000
Tool/software: WEBENCH® Design Tools
Dear Sir,
We were working on power line communication with thvd 8000 for our application. Thvd totally works on Rs485 interface with the mcu. But my question is while am using 2 evm of thvd i want to transmit data to another board over the power bus line.
vbb and gnd will be the input supply on the bus line and taking forwarded to other nodes.?
vcc and gnd are the input for thvd 8000 IC,But eventually we have to take power line bus connected with other nodes and transfer data that will be vbb and gnd.?
But eventually we have to take power line bus connected with other nodes and transfer data
Below link Page 6 (3.2 Operation Example)

2. (Optional) Connect Vbb and GNB through Vbb and GNB connectors for power delivery. Short the shunt TL_A and TL_B to connect the inductor to bus. The maximum DC current rating of the populated inductor on the EVM is 1.9 A. The voltage rating of the populated capacitor is 100 V. On the transmitting board, Vbb and GNB connect to the power source, like a 12 V DC. On the receiving board, Vbb and GNB connect to the loading circuit (Figure 1). The received power may have a lower voltage level due to the cable loss.
am not getting the Jumper setting of inductor with the bus for evm.