This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Instalation Problem

Hi

I am trying to instal the SwitcherProDTSetup.msi  to my system,

but  i am getting the message as

THE SETUP REQUIRES THE .NET FRAMEWORK VERSION 3.5,PLEASE INSTAL .NET FRAMEWORK AND RUN THIS SETUP AGAIN.

Then i instaled the

dotNetFx35setup.exe from  http://www.microsoft.com/downloads/en/details.aspx?FamilyId=333325fd-ae52-4e35-b531-508d977d32a6&displaylang=en

and NETCFSetupv35.msi from http://www.microsoft.com/downloads/details.aspx?FamilyID=e3821449-3c6b-42f1-9fd9-0041345b3385

but after that also i am getting the same erroe please let me know which file i need to instal to solve this error

Thanks in advance

rangareddy

  •  

    Hey Ranga,

    Did you reboot your computer after installing .NET FRAMEWORK VERSION 3.5 ? 

    Thanks,

    Vaibhav

  • yes i did,, but now also i am getting the same error

  • Hi Ranga,

    If you don't mind me asking, why are you installing the software from SwitcherProDTSetup.msi and not from SwitcherProDTSetup.exe?
    SwitcherProDTSetup.exe should automatically download and install all dependencies for you. SwitcherPro actually has two dependencies:

    1) dotnetfx.exe (from 'http://go.microsoft.com/fwlink/?LinkId=37283'). 3.5 is the minimum .NET. I highly recommend the latest-and-greatest from MS.
    2) SSCERuntime-ENU-x86.msi (from http://go.microsoft.com/fwlink/?LinkId=115207&clcid=0x409). This is the SQL engine that SwitcherPro uses.

    But, downloading and installing these manually is not required on a correctly configured Windows XP SP3 or Windows 7 host that has an internet connect. What version of Windows are you using?

    Also, please delete the contents of C:\Document and Settings\<userid>\Local Settings\Temp before you start the installation. If the install fails, you should find a log in this directory. Please post the contents of the log if you continue to experience problems.

    Thanks,
    Michael

    -- 
    Michael Krasnicki
    Analog eLab
    Texas Instruments
  • THIS IS THE CONTENT OF LOG FILE  PLEASE CHECK IT..

     

    The following properties have been set: Property: [AdminUser] = true {boolean} Property: [ProcessorArchitecture] = Intel {string} Property: [VersionNT] = 5.1.2 {version} Running checks for package 'Windows Installer 3.1', phase BuildList The following properties have been set for package 'Windows Installer 3.1': Running checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' Result of running operator 'VersionGreaterThanOrEqualTo' on property 'VersionMsi' and value '3.1': false Result of running operator 'ValueExists' on property 'Version9x': false Result of running operator 'VersionLessThan' on property 'VersionNT' and value '5.0.3': false Result of running operator 'ValueNotEqualTo' on property 'ProcessorArchitecture' and value 'Intel': false Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false Result of checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' is 'Install' 'Windows Installer 3.1' RunCheck result: Install Needed Running checks for package '.NET Framework 3.5 SP1', phase BuildList Reading value 'SP' of registry key 'HKLM\Software\Microsoft\NET Framework Setup\NDP\v3.5' Unable to read registry value Not setting value for property 'DotNet35SP' The following properties have been set for package '.NET Framework 3.5 SP1': Running checks for command 'DotNetFX35SP1\dotNetFx35setup.exe' Skipping ByPassIf because Property 'DotNet35SP' was not defined Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false Result of running operator 'VersionLessThan' on property 'VersionNT' and value '5.1.2': false Result of running operator 'VersionEqualTo' on property 'VersionNT' and value '5.2.0': false Result of running operator 'ValueEqualTo' on property 'ProcessorArchitecture' and value 'IA64': false Result of checks for command 'DotNetFX35SP1\dotNetFx35setup.exe' is 'Install' '.NET Framework 3.5 SP1' RunCheck result: Install Needed Running checks for package 'SQL Server Compact 3.5', phase BuildList Reading value 'DesktopRuntimeVersion' of registry key 'HKLM\SOFTWARE\Microsoft\Microsoft SQL Server Compact Edition\v3.5\ENU' Unable to read registry value Not setting value for property 'ENU_INST' Reading value 'System.Data.SqlServerCe.dll_ENU' of registry key 'HKLM\SOFTWARE\Microsoft\Microsoft SQL Server Compact Edition\v3.5\GAC' Unable to read registry value Not setting value for property 'ENU_INST_GAC' The following properties have been set for package 'SQL Server Compact 3.5': Running checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi' Skipping ByPassIf because Property 'ENU_INST' was not defined Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false Result of checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi' is 'Install' Running checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi' Skipping ByPassIf because Property 'ENU_INST' was not defined Result of running operator 'ValueExists' on property 'ENU_INST_GAC': false Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false Result of checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi' is 'Install' 'SQL Server Compact 3.5' RunCheck result: Install Needed EULA for components 'Windows Installer 3.1' was accepted. EULA for components '.NET Framework 3.5 SP1' was accepted. EULA for components 'SQL Server Compact 3.5' was accepted. Copying files to temporary directory "C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\" Downloading files to "C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\" (11/7/2010 4:17:38 PM) Downloading 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' from 'http://go.microsoft.com/fwlink/?LinkId=49256' to 'C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\' Download completed at 11/7/2010 4:17:39 PM Verifying file integrity of C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe WinVerifyTrust returned -2146762749 Subject form unknown (11/7/2010 4:17:39 PM) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\' Download completed at 11/7/2010 4:17:39 PM Verifying file integrity of C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\DotNetFX35SP1\dotNetFx35setup.exe WinVerifyTrust returned -2146762749 Subject form unknown (11/7/2010 4:17:39 PM) Downloading 'SQL Server Compact Edition\SSCERuntime-ENU.msi' from 'http://go.microsoft.com/fwlink/?LinkId=115207&clcid=0x409' to 'C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\' Download completed at 11/7/2010 4:17:41 PM Verifying file integrity of C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\SQL Server Compact Edition\SSCERuntime-ENU.msi WinVerifyTrust returned 0 File trusted Running checks for package 'Windows Installer 3.1', phase BeforePackage The following properties have been set for package 'Windows Installer 3.1': Running checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' Result of running operator 'VersionGreaterThanOrEqualTo' on property 'VersionMsi' and value '3.1': false Result of running operator 'ValueExists' on property 'Version9x': false Result of running operator 'VersionLessThan' on property 'VersionNT' and value '5.0.3': false Result of running operator 'ValueNotEqualTo' on property 'ProcessorArchitecture' and value 'Intel': false Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false Result of checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' is 'Install' 'Windows Installer 3.1' RunCheck result: Install Needed Verifying file integrity of C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe WinVerifyTrust returned -2146762749 Subject form unknown Error: Setup has detected that the file 'C:\DOCUME~1\RANGAR~1\LOCALS~1\Temp\VSDE51.tmp\WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' has changed since it was initially published.

  • Hi Ranga,

    According to your log, you are running Windows XP Service Pack 2. The installer is looking for a bunch of registry settings that don't appear to exist on your machine, most likely because you are running SP2. To fix your problem, you will need to update to Windows XP SP3. Please use http://update.microsoft.com to update your computer or download SP3 at "http://www.microsoft.com/downloads/en/details.aspx?FamilyID=5b33b5a8-5e76-401f-be08-1e1555d4f3d4&displaylang=en". You may also need to reinstall/patch .NET after updating to SP3.

    Regards,
    Michael

    -- 
    Michael Krasnicki
    Analog eLab
    Texas Instruments

     

  • if I install MSP-GANG software on 64 bit PC,what shoud i do? The "WindowsInstaller3_1 " contain a exe for x86, and which file should i download?