Tool/software: WEBENCH® Design Tools
Hey all,
I have a customer that is looking for a low cost buck converter that can take a 23 V input and output 1.2 V @ 200 mA. I'm recommending the the TPS560430 for his applications but I tried simulating on Webench using the following specs; Vin: 8-36V, Vout:1.2V, Iout:0.2mA and ambient temp:30C and the design pops up that it cannot be created. All of these are within the operating specs of the device so is there an issue with Webench? Thanks for the help
-Stephen