Part Number: LM5023
Tool/software: WEBENCH® Design Tools
Hi
I did a design using the LM5023 controller on Webench and everything is clear to me apart from the Primary winding construction detail.
The instructions are as follow..
What I am unclear about is the following. Are the two Primary windings in Parallel, ie. starts on the same pin, eg. pin 1 and ends on the same pin, eg pin 3? I am unclear as to the meaning of the 2/4.0 number.
Your help will be appreciated as I need the transformers wound to test the prototypes.
Best regards
Chris