Hello
I wonder how the primary Cr module/secondary Cr modules are placed on the board. The assembly is not clear, it is appearing in the layout that the capacitors are into the magnetic core of the transformer, would appreciate some clarification regarding the assembly.
The connection is not clear also; according to the schematic design note:
9. Net Leg_1_Prim and Crp_1 are shorted via boards to XFMR pin connections
10. Net Leg_1_Sec and Crs_1 are shorted via boards to XFMR pin connections.
Thanks in advance