Hi team,
Can you please help with below queries?
Sno. |
Page no. |
Section |
Sub Section |
Doubt |
1 |
13 |
3.2 |
Figure 15 |
Please clarify if all the mentioned ‘R’ are equal for the load card. And suggest the value and rating of the same. |
2 |
26 |
3.2.5 |
Para below Fig. 40 |
"When only S2 is closed, the Viso-Vref voltage is confirmed to be across Rns1, Rns2, and Riso, which can be measured from ISO_NEG." |