Hi,
I generated pulse in another tool and imported the waveform as pwl file in voltage generator.
What should be the series resistance value for this voltage generator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I generated pulse in another tool and imported the waveform as pwl file in voltage generator.
What should be the series resistance value for this voltage generator?
Hi Bhavya,
Thanks for reaching out to TI.
There are many pulses defined in the automotive standard ISO 7637-2 and most of them have different series resistor (Ri) values. I would recommend you to refer to the ISO 7637-2 standard understand the various test pulses and their test requirements. Thanks.
Regards,
Koteshwar Rao
As per the standard series resisor to be added is 10 ohms. When I added this value to voltage generator, the output is not coming properly
Hello Bhavaya,
Thank you for your inquiry about TINA. Since TINA is a DesignSoft/TINA program, questions are handled by using the DesignSoft support page: http://www.tina.com/technical-support/ .
The DesignSoft/TINA team is very helpful and this is the most direct way for TINA support. Please advise by Reply when the issue has been resolved.
Regards,
~Leonard