Hi,
I am working with a customer who is using our TMUX1309 model available at TI.com. When I was trying to troubleshoot the issue - the model was not in the PSpice for TI library. However on colleagues computers it is - please see below for reference:
My Version:
Colleagues Version:
I have tried re-installing the PSpice libraries by using the help menu to no avail. I also uninstalled PSpice for TI and reinstalled it and still no updated libraries. I even tried to re-install from my new installation. I've also tried deleting the metadata and reinstalling - it keeps pulling a file from 1/13-14/21, so I am not sure if this is the right data it is pulling or not.
Any help is greatly appreciated because due to the limit on importing models I can't perform the needed simulations for a TI PSpice model.
Best,
Parker Dodson