Part Number: TIDA-01093
Other Parts Discussed in Thread: ISO1541, ISO1540, BQ76930
Dear TI,
Please refer below image , which is of datasheet.
It shows Input side current consumption by chip .

According to that if i connect Upper _ Afe Reg_Out as a voltage source to power up secondary of Chip , than in situations when 198mA current is required by I2c Chip , AFE would not be able to deliver, please share is it ok to go in such a way of connection ?
I mean can Upper AFE Reg out be used to power up I2c Isolator?
Please comment .
Rohit