Part Number: PMP8928
Other Parts Discussed in Thread: TPS40170, LM5145
Hi team,
Do we have XY coordinate file could be shared?
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
I see that the gerbers are available in the tool folder, but no XY placement data.
By the way, the LM5145 is preferred over the TPS40170. It has the same control loop (voltage mode) parameters. Here is an IBB quickstart calculator - please edit as needed:
LM5145 IBB Quickstart r1, VIin= 12V, Vout = -48V, Iout = 4A, Fsw = 250kHz.xlsm.
Regards,
Tim
Hi Tim,
Because PMP8928 is ready. We would like to make board by ourselves.
We need the XY placement file for the component surface mounting. Could you provide the layout original file? We can get the XY placement data from it.
Regards,
Roy
Hi Roy,
Here are the Altium source files for PMP8928:
PMP8928 REVA (7-13-2021 8-13-54 AM).zip
Regards,
Tim