Part Number: TIDA-00317
Hello,
i've made a liquid level sensor following your "TIDA-00317" reference design. The sensor is placed on a custom PCB that is glued to the container wall (2mm plastic).
If there is water in the container, the sensor works very well. However, the sensor should measure a fluid that sticks a bit to the wall. When the container is filled for the first time, the measured level rises correctly, but after the container is emptied, the measured capacity remains the same as when the container is full, because a film about 1mm thick remains on the wall.
Is there a way to change the design of the sensor so that the 1mm film does not affect the measurement?
Thanks,
Florian