Other Parts Discussed in Thread: UCC28880, UCC28911, UCC28910
Hi,
Customer is working on a design based on PMP10143, according to them it is working very well.
However,their load is only 250mA on 3.3VDC causing a Fsw of about 4.5kHz which is audible. By modifying C9 for 10nF and R5 for 4.7K, they've been able to raise the Fsw to 9.3kHz which is better.
Now they wondering if there is a way to raise it more without too much modifications, ideally over 20kHz. Do you have an almost drop-in replacement controller which have a fixed frequency but adjustable PWM?
Regards,
Maynard