Part Number: TIDA-010210
about the used Power Half Bridges Designs in reference "TIDA-010210"
XTIDA-ANPC-DC1 , XTIDA-ANPC-DC2 , XTIDA-ANPC-DC3
the three legs have approximately the same power ratings of power switches 600V & about 35A
Is their any limitation to use them in a design and get output current of 16-A from each leg.
In the Main Design "TIDA-010210" the output current is 10-A (on AC side). what is limiting that current from getting higher?
Is it related to the system design?
or limited to the layout design itself?
If it isn't the layout design limitation ? and each leg can deal with higher current ratings, what are the limits ?
thanks