Other Parts Discussed in Thread: TPS562202
Dear Commnity,
I am trying to simulate the TPS562202 module in Pspice for TI with parametric analysis for feedback resistor tolerance of 1%.
I am getting below error while simulating.
Kindly let me know what could be the reason.
----ERROR---
Starting GMIN stepping
Starting power supply stepping
Starting pseudo-transient algorithm
INFO(ORPSIM-16594): To improve Pseudotransient Convergence and Performance, set following options to relax stabilization criteria for capacitor currents and inductor voltages: PTRANABSTOL=1e-5, PTRANVNTOL=1e-4
WARNING(ORPSIM-16534): Using high values of ITL4 for Speed Level > 0 may increase total simulation job time.
Convergence problem in DC sweep
These voltages failed to converge:
V(X_U1.U5_U18_N15541459) = 1.685uV \ 369.28nV
V(X_U1.U5_U18_N15541111) = 4.214uV \ 369.28nV
V(X_U1.U5_U18_N16295604) = -1.635uV \ 832.96nV
V(X_U1.U5_U18_CDIFF) = -2.468uV \ 8.411pV
V(X_U1.VOINFO) = 6.277uV \ 369.27nV
ERROR(ORPSIM-15661): 5 of 5 errors shown. See output file for complete list
These supply currents failed to converge:
I(X_U1.E_U5_E1) = 22.47pA \ -2.536pA
I(X_U1.E_U5_U13_E1) = -24.51pA \ -2.150e-18A
I(X_U1.X_U5_U13_F1.VF_U5_U13_F1) = 24.51pA \ 2.150e-18A
I(X_U1.X_U3_U580.v1) = 93.83uA \ 5.000A
I(X_U1.X_U3_U580.v2) = 666.57nA \ 1.035pA
ERROR(ORPSIM-15660): These devices failed to converge
X_U1.X_U3_U580.d_d10
INFO(ORPROBE-3185): Simulation paused
INFO(ORPROBE-3183): Simulation running...
ERROR(ORPSIM-16551): Floating point computation failed during Device/Model Load. Possible solutions: 1)Ensure that all device parameters are in valid range. 2)Try using .options LIMIT
Divide by Zero in device X_U1.X_U3_U580.d_d11, Divide
INTERNAL ERROR -- Divide by Zero in device X_U1.X_U3_U580.d_d11, Divide
Run aborted
Thanks & Regards,
Preethi