in page 16, what's Vload_detect, how to get this value?
in page 25, 3.2.2.4 Standby Mode
The battery pack in the first scenario should be able to detect if the charger is attached or if the battery pack is put inside of the e-bike. The battery pack in the second scenario should be able to detect if load is on or if the battery pack is plugged in outside of the e-bike.
The first pulse of PMON is to measure PACK voltage with pre-discharge MOSFET off. If the charger is attached, the voltage should be equal to 54.6 V. If not, the pre-discharge will be turned on. After a short time delay, the PACK voltage will be measured again. If the battery pack is put in the e-bike, a large capacitor will be connected between PACK+ and PACK-, therefore, the measured voltage is lower than the battery voltage. Otherwise, the PACK voltage is equal to the battery voltage.
Does the large capacitance refer to the starting capacitance of the controller? why the measured voltage is lower than the battery voltage? but i think It takes a very short time for the capacitor to be fully charged,the capacitor's voltage is close to battery voltage.How long is the sampling time? t=RC=302*C
Otherwise, the PACK voltage is equal to the battery voltage. The battery is placed outside the bicycle. The measured voltage is the voltage of Pack + and pack - after C71 and C70 are charged? is right?
. In the second scenario, the pre-discharge MOSFET is mostly on. If load is on, there will be a voltage drop across the resister series with the pre-discharge MOSFET, therefore, the measured voltage is lower than the battery voltage. If not, the pre-discharge will turn off. After a some time delay, the PACK voltage is measured. If the battery pack is plugged outside of the e-bike, the output capacitor is much smaller, which will cause a larger voltage drop.
i do not understand "if not"meaning? If not, the pre-discharge will turn off. After a some time delay, the PACK voltage is measured. If the battery pack is plugged outside of the e-bike, the output capacitor is much smaller, which will cause a larger voltage drop. "plugged outside of the e-bike" if the battery is outside the bicycle, because the turn off the pre-discharge, the pack voltage i think it should 0V.