Other Parts Discussed in Thread: BQ76952,
Hello
I like the PACK and LD sensing circuit Ryan Tan has used (whole Sch uploaded) but I have changed to a 64V bidirectional TVS across the PACK terminals. By adjusting R141 and R142 to 1/4W, I believe the circuit will handle continuous charge voltage reversal (to -65V) so safety does not rely on current limiting on the charger.
My question is:
The data sheet shows effective input resistance of LD and PACK pins [R (ADC_IN_LD) and R (ADC_IN_DIV)] of 2Mohm and 600Kohm respectively.
We can calibrate away the resistance of the external sense circuit at manufacturing (single temperature) but I am interested in modelling the circuit to decide if we can select resistor tempco to act with the tempco of the divider in the BQ76952 to optimise measurement accuracy over pack temperature. This is for autonomous operation or where temperature compensation is not practical.
In another post, Matt Sunna has directed me to the pin equivalent circuit document, sluaaf2.pdf, which is a guide but I would need a graph of effective input resistance over temperature. Is this data that the design team has available ?
All the best
Harry