This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01487: Problem with 2 repeater on a bus

Part Number: TIDA-01487

Hi, in my application i use 1 TIDA-01487 circuit to insulate 1 node of bus. the bus has 4 node and works fine. I can monitor the bus with CANKing and the error counter is zero.

If i use 2 TIDA-01487 to isolate a second node i get a series of errors of the bus which seems to be due to unmanaged conflicts.

Is possible to use more than one TIDA-01487 at the same bus?