Hi,
Like the title says, the software systematically crashes whenever I try to edit or create a new profile in a project.
I must specify that when I'm working locally on my hard drive everything works fine. The crashes happen when the location of the project itself is on a shared disk we use and for which I have all the access right needed. The project launches normally, I can even run simulations associated with already existing profiles but I cannot modify them and I cannot create new simulation profiles.
I have colleagues that have encountered the same issue and others for which everything works fine in all possible configurations (local, remote project, adding libraries and symbols from third party ect).
Thx in advance for your help,
Claudio