Part Number: TIDA-010054
Hi Harish,
To design a DAB converter I am using the reference design TIDA-010054. The specifications are as below
Input 250 to 425V
Output - 10.5 to 15.5V
Output Power - 2400W
Fsw - 100kHz
I tried to use the formulas provided in the reference design for calculating leakage inductance, peak primary current. etc.
For leakage inductance calculation I am using below formula

Here N should be primary to secondary ration or secondary to primary turns ratio?
For primary peak current I am using below formula

In this n should be primary to secondary turns ratio or secondary to primary turns ratio?