Part Number: TIDA-050017
Other Parts Discussed in Thread: LM73606, LM61480, TPS55288, LM5175
Hello,
i am designing a TEC controller based on dc-dc converters, similarly to what is reported in TIDA-050017. I would like to ask for some info about the following points.
1) For this purpose I am trying to identify a 2-quadrant buck converter with the following (general) characteristics:
- type: buck/buck-boost/synchronous buck
- current capability > 4.5 A both in sourcing and sinking (2-quadrant operation)
- price < 3 USD
- output voltage range: 1 V to 12 V minimim
- external inductor/internal switches are preferred (converters)
Are there some parts from TI which could be a match?
2) I was taking a look at TI products to see whether I could find a synchronous buck with sufficient current sinking capability, in order to be able to reverse the TEC current. The current needed during cooling is generally greater than the one needed for heating, but I was trying to identify a component with sufficient balancing between maximum sourcing and sinking current capability.
2a) In this regard, the LM61480 and LM73606 are reported to have a -5.3 A and -5 A sink limit, respectively. Could these ICs be a match for the stated application?
2b) Are there any parts like the TPS6307x, but capable of handling greater currents in sourcing and sinking? For example the TPS55288 could be a candidate, but no reverse current limits are specified on the datasheet.
3) Another solution I was investigating was to use a 4-quadrant converter like the LT8714 from AD in order to have bipolar regulation on a single output. Are similar solutions available from TI?
Thanks for your help and best regards,
DP