Part Number: TIDA-050047
Other Parts Discussed in Thread: TPS25750, BQ25790, BQ25792
Hi,
I tested the current consumption for the TIDA-050047 at idle (no load). The result was more than expected. The multimeter showed about 67 mA. From which component is so much current drawn? And why does the temperature of the charger rise up to 45° degrees when idle.
Thank you in advance
Regards,
Hussein