Dear sir ,
We have designed a charger of specs 69.2V,4A (72.8 V OVP)
When I am connecting a load resistance of 14 ohms , 17.5 ohms,28 ohms the output voltage comes out to be < 43 V (output voltage below which charging current is CC/10) while the charging current is 0.4A and the output of CC loop controller (2.67) comes out to be less than output of CV loop controller (9.6V) as expected . But when I am connecting the battery terminals having initial voltage (53V) the charging current comes out to be 3.5 A instead of 4A also output of both CC and CV loop controller comes out to be high (9.6V) also I have set IREF to be 1V but IOUT_FB at inverting terminal (6) of TL103 comes out to be 0.911 V instead of 1V (When CC=0.4 A IREF=0.1V= IOUT_FB ) .
(1) Why reference is not meeting the feedback value when battery load is connected ?
(2) is it possible that any parameter is limiting the CC Current to reach 4A because CC Controller output is high so it has to reach 4A to meet IREF=IOUT_FB ?