Other Parts Discussed in Thread: PSPICE-FOR-TI, TLV3601
Hi, i realize TI will not directly answer questions re: model operation in LTspice. I am waiting for approval from my IT office to install PSPICE-for-TI... in the meantime i'm doing some simulation in LTspice. I created a model for the TLV3601 from the 'tlv3601.lib' but the output is not performing as expected. I'm operating from a 2.4VDC supply... with the input conditions, i expect to see output pulses from 0 to 2.4VDC, however the output is sitting on a VCC/2 bias and the pulse amplitude is millivolts (see attached image).
The below comment appears at the beginning of the .lib file:
* INCORRECT INPUT CONDITIONS: If an error condition occurs, such as
* incorrect supply voltages or exceeding input voltage range, the output will go to
* half the supply voltage. The real device will NOT do this.
I think this may have something to do with the erroneous results i'm seeing? the fact that the output IS switching at the expected times, just not at the correct amplitude, leads me to believe it's working. albeit with this issue. My inputs are within the range specified in the datasheet. Does anyone know if this is in fact a problem with the model code? can this be fixed?
thanks in advance,