This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01017: MMWCAS-DSP-EVM + MMWCAS-RF-EVM cascade radar application with linux.

Part Number: TIDEP-01017
Other Parts Discussed in Thread: MMWCAS-RF-EVM

Hello!

I use MMWCAS-DSP-EVM + MMWCAS-RF-EVM in cascade radar mimo application with network connection to another board.
In cascade_radar_object_detect uscase cfg.mk file configurated to use IPU(01 and 11), dsp1, eve1-eve4. MPU core is not used, but i want to use it to do some calculations and data transfer.
How can i use MPU with linux core for calculation and network transfer?