This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP4448: Design suggestion to use TPS92314

Part Number: PMP4448
Other Parts Discussed in Thread: TPS92314

My requirements are more or less the same as the PMP4448 reference design. Unfortunately, the availability of the TPS32914A is very poor. Is there a possibility to realize the design with the TPS92314 (not A-Type)?

My requirements are:

Vin typ. 100...240VAC (85...265VAC)
Vout approx. 36V
Iout 240mA
Non-Dimmable / Non-Isolated / Buck (with simple inductor)