Part Number: PMP20742
Hi,
I noticed that the PMP20742 design uses 100 µF 25 V polymer for C15. What is the reason behind using a polymer cap instead of an electrolytic cap? If possible, we would like to use an electrolytic instead.
Thank you,
Sith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP20742
Hi,
I noticed that the PMP20742 design uses 100 µF 25 V polymer for C15. What is the reason behind using a polymer cap instead of an electrolytic cap? If possible, we would like to use an electrolytic instead.
Thank you,
Sith
Hi Sith,
Yes, an electrolytic capacitor can be used instead of a polymer for C15.
thanks,
Brian