Part Number: PMP7899
Hi,
Can we upgrade the design for 48V 1.4A
The input would be 12V dc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Akash,
This would be increasing the power 40%, it is certainly possible, but the transformer would need to change, the FET, input capacitors and output capacitors would all need to upgraded.
Hopefully this helps.
Thanks,
Robert