Part Number: TIDA-010054
Hi TI,
Input (coming form Vienna rectifier) 700 to 800 V
output power - 50KW
How Can I achieve the 50KW at the out put power and how to select leakage inductance and transformer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010054
Hi TI,
Input (coming form Vienna rectifier) 700 to 800 V
output power - 50KW
How Can I achieve the 50KW at the out put power and how to select leakage inductance and transformer
Hello,
The selection of leakage inductance and transformer depends on the output power, max input/output voltage and SW freq. The details of leakage inductance design can be found from our design guide page 22 equation 18. Pls note that N is the sec to prim turn ratio, which is 0.625. The transformer is the custom design based on the spec from page 28.
The link of design guide: www.ti.com/.../tidues0

Regards
Lei