Other Parts Discussed in Thread: TIDA-00777,
Hi Guys,
1. It is mentioned in the application note ( TIDUBV4A) that Self resistance, Inductance, and capacitance of the Rogowski coil is 0.77ohms, 8.34uH & 7.56pF but whereas when I measure from my network analyzer the resistance value comes around few 11-15ohms, and the capacitance value also does not match. could you please let me know your measurement procedure?

2. Instead of using a digital integrator I have tried to use an analog integrator (similar to TIDA-00777) but the waveform I get is very noisy as shown below, is there any method to reduce the noise?

Frequency - 200Hz, Current - 24A (RMS) ----- Yellow- output of the analog integrator || Orgage- is the FFT of the output